Technical FAQs

Ask a Question

Which ports do Vijeo Designer use during a download?

Goals and Symptoms

Which ports do Vijeo Designer use during a download?

Causes and Fixes

During the download to a target through Ethernet (Runtime Installer and/or download of an application), it uses TCP ports 6001 and 13777. We used port 21 instead of 6001 in the past but, since Vijeo-Designer 4.3.0, we use port 6001.


Legacy KB System (APS) Data: RESL181179 V1.0, Originally authored by on , Last Edited by MaMi on 01/09/2007
Related ranges: Vijeo Designer
Was this helpful?
What can we do to improve the information ?