Technical FAQs

Ask a Question

What are the dimensions for the XBTGT protections sheets (XBTZG61, XBTZG62, XBTZG64, XBTZG65, XBTZG66 and MPCYK50SPAKIT)?


TERMINAL REFERENCE SIZE (in mm)
***************************************************************
XBTGT1100 XBTZG61 126 x 99.9
XBTGT1130
***************************************************************
XBTGT2110 XBTZG62 131.4 x 159.4
XBTGT2120
XBTGT2130
XBTGT2220
XBTGT2330
***************************************************************
XBTGT4230 XBTZG64 166 x 210
XBTGT4330
XBTGT4340
***************************************************************
XBTGT5330 XBTZG65 205 x 255
XBTGT5340
***************************************************************
XBTGT5230 XBTZG66 231 x 298
XBTGT6330
XBTGT6340
***************************************************************
XBTGT7340 MPCYK50SPAKIT 236.7 x 312.7


Legacy KB System (APS) Data: RESL179170 V1.0, Originally authored by on , Last Edited by on
Related ranges: Magelis XBT GT
Was this helpful?
What can we do to improve the information ?