Technical FAQs

Ask a Question

What would cause a GPF (General Protection Fault) when trying to install ProWORX Nxt SR6 (Service Release 6)?

The most common cause for this error is not having the Nxt220s6.exe in the same folder as nxt.exe. To resolve the issue, move the Nxt220s6.exe into the same folder as the nxt.exe which is usually the nxt folder.


Legacy KB System (APS) Data: RESL175065 V1.0, Originally authored by on , Last Edited by on
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?