Technical FAQs

Ask a Question

What Ethernet frame types are supported by the TSXETG1010 module?

The Ethernet frame types that are supported by the TSXETG1010 module are:
Ethernet II format, corresponding to standard RFC 894 (the most commonly used) and
802.3 format, corresponding to standard RFC 1042.


Legacy KB System (APS) Data: RESL174655 V2.0, Originally authored by MiOB on 07/30/2013, Last Edited by GeMc on 07/30/2013
Related ranges: Modicon Atrium
Was this helpful?
What can we do to improve the information ?