Technical FAQs

Ask a Question

What protocols are supported by the TSXETG1010 module?

The following protocols are supported by the TSXETG1010 module.
UNI-TEL (by default)
MODBUS


Legacy KB System (APS) Data: RESL174651 V2.0, Originally authored by MiOB on 07/30/2013, Last Edited by GeMc on 07/30/2013
Related ranges: Modicon Atrium
Was this helpful?
What can we do to improve the information ?