Technical FAQs

Ask a Question

How to download the Vijeo Designer application to the CF (compact flash) card on the PC.

Goals and Symptoms

To download the Vijeo Designer application to the CF card

Facts and Changes

Vijeo Designer V4.2

Causes and Fixes



Then fill the path to transfer to the CFcard. (example : « G:/ », it depends on your PC)

Once the transfer is complete, insert your CFcard in the XBT-G.

Dont forget to put the switch number 1 at ON (to start from the CFcard and not from the internal memory). Your runtime will be automatically run if using
V4.2 of the software.


Legacy KB System (APS) Data: RESL173976 V2.0, Originally authored by MiOB on 08/07/2013, Last Edited by GeMc on 08/07/2013
Related ranges: Vijeo Designer
Was this helpful?
What can we do to improve the information ?