Technical FAQs

Ask a Question

Is it possible to change the communication port address of a Twido controller without using TwidoSoft?

Yes, there are two possible solutions:
1. Using the local display (TWD XCPODC or TWD XCPODM).
2. System bits and words method: to use this method follow the sequence below:

Sequence
- Set the system bit %S101 to 1
- Change the address values of the communication ports.
%SW101 for port 1
%SW102 for port 2
- Set the system bit %S101 to 0, at that time, the system will take into account the new addresses,
apply instantly the changes, and save the data into the configuration part of the application.


Legacy KB System (APS) Data: RESL173971 V2.0, Originally authored by MiOB on 05/02/2013, Last Edited by GeMc on 05/02/2013
Related ranges: Twido
Was this helpful?
What can we do to improve the information ?