Technical FAQs

Ask a Question

What is the maximum current draw of the TwidoPort?

The maximum current draw is 180 mA @ 5 VDC.


Legacy KB System (APS) Data: RESL173970 V2.0, Originally authored by MiOB on 08/07/2013, Last Edited by GeMc on 08/07/2013
Related ranges: Twido
Was this helpful?
What can we do to improve the information ?