Technical FAQs

Ask a Question

Can I have two Premium PLCs I/O scanning to a single Advantys Ethernet NIM?

Yes, in read only. However only one IO Scanner at a time is allowed to access the Advantys NIM in write mode.

Legacy KB System (APS) Data: RESL173500 V2.0, Originally authored by MiOB on 07/19/2013, Last Edited by GeMc on 07/19/2013
Related ranges: Modicon Premium
Was this helpful?
What can we do to improve the information ?