Technical FAQs

Ask a Question

What's the difference between the .DBF and .DIF spreadsheet files when importing/exporting them in the ProWorx NxT software?

A *.DBF file will export/import the descriptors and short comments.
A *.DIF file will export/import the descriptors, short comments along with page titles and long comment numbers.

Legacy KB System (APS) Data: RESL170420 V1.0, Originally authored by on , Last Edited by on
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?