Technical FAQs

Ask a Question

What is the difference between Concept S, M and XL?

The main difference is the PLCs that are supported by each package they support. Here are the ordering part numbers for the latest Concept v2.6 software and support information.

372SPU47101V26.....Concept S v2.6 Package. The Small offering designed to program Momentum PLC applications only. Programming languages include 984 LL, LD, FBD, IL, but not SFC.
 
372SPU47201V26.....Concept M v2.6 Package. The Medium offering is designed to program Momentum and Compact 984 PLCs. It supports 984LL and all IEC Programming Languages.

372SPU47401V26.....Concept XL v2.6 Package. The full feature package programs Momentum, Compact 984, and Quantum.
It supports all IEC programming languages as well as the inclusion of extended block libraries in the areas of analog I/O XMIT communications.

Note: Concept only supports the high end Compact 984 E258/265/275/285 PLC's.
 

text text
 
Was this helpful?
What can we do to improve the information ?