Technical FAQs

Ask a Question

Is the VAMP 321 CSA listed?

Yes, the VAMP 321 is CSA and UL listed.


Legacy KB System (APS) Data: RESL213091 V1.0, Originally authored by DaFr on 12/06/2013, Last Edited by DaFr on 12/06/2013
Related ranges: Others protection relays

AEDL3
Was this helpful?
What can we do to improve the information ?