Technical FAQs

Ask a Question

ADVC Loop Automation rules for Feeder, Mid-Point, and Tie

The ADVC allows for three different types of configurations for Loop Automation. Each of these configurations may behave differently and may have a different action given a certain event. These rules are detailed below:


Legacy KB System (APS) Data: RESL213081 V1.0, Originally authored by DaFr on 12/05/2013, Last Edited by DaFr on 12/05/2013
Related ranges: Others protection relays

AEDL3
Was this helpful?
What can we do to improve the information ?