Technical FAQs

Ask a Question

When opening a Centurion MJR file in WSOS5 an error occurs

If only one file is present, typically the .sos file, WSOS5 will produce an error when opening the file as two additional files are needed. The other two files will have the same name with different extensions. These other extensions are .rm5 and .rmt. All three files must be in the same directory for the software to open the switchgear file. Below is the error message;


Legacy KB System (APS) Data: RESL212982 V1.0, Originally authored by DaFr on 11/08/2013, Last Edited by DaFr on 11/08/2013
Related ranges: Others protection relays

AEDL3
Was this helpful?
What can we do to improve the information ?