Technical FAQs

Ask a Question

What is the waveform resolution for the Sepam relays?

The Sepam 20 and 40 series relays offer 12 samples/cycle resolution for the waveforms.
The Sepam 80 series relays offer 36 samples/cycle or 12 samples/cycle, configurable on the FRT screen in SFT2841.


Legacy KB System (APS) Data: RESL212946 V1.0, Originally authored by DaFr on 11/05/2013, Last Edited by DaFr on 11/05/2013
Related ranges: Sepam series 20

AEDL3
Was this helpful?
What can we do to improve the information ?