Technical FAQs

Ask a Question

How to perform a file comparison for the ADVC controllers using WSOS5

WSOS5 offers a file comparison feature which will compare the Switchgear file that is loaded into WSOS and the Switchgear file which is loaded into the controller itself. In order to perform this comparison open a switchgear file with WSOS5 and place an ADVC controller online (Options > Go On-Line). Once this is done click Options > Compare Switchgear Settings, this will display a menu that allows the selection of what you would like to compare (Protection, Telecontrol, Operator, IOEX Mapping, Protocol Mapping, Quick Key Mapping, and VT Configurator).


Legacy KB System (APS) Data: RESL212732 V1.0, Originally authored by DaFr on 10/11/2013, Last Edited by DaFr on 10/11/2013
Related ranges: Others protection relays

AEDL3
Was this helpful?
What can we do to improve the information ?