Technical FAQs

Ask a Question

Some DNP mapping numbers are red when viewed from WSOS5 DNP configurator

You may find red numbers within the DNP map, this implies that the range associated with the index (typically Analog) is out of range. Within the DNP mapping configurator (located at the top of the map configurator) is an option for 16-bit or 32-bit. Verify that this setting is correct and adjust the range for the index if necessary.


Legacy KB System (APS) Data: RESL212730 V1.0, Originally authored by DaFr on 10/11/2013, Last Edited by DaFr on 10/11/2013
Related ranges: Display for Protection Relay PRODUCTS
Was this helpful?
What can we do to improve the information ?