Technical FAQs

Ask a Question

When attempting to place an ADVC controller online using WSOS an error message is displayed in the lower right-hand corner "On-line - Communication Fail."

This error message indicated that the communications to the ADVC controller are not configured correctly. To configure these parameters, click options > Go Offline (it never went online but the software will continue trying until manually stopped) then click on Customize > WSOS Communications > Click the tab that described the method which you are using for communications and configure it accordingly. Most commonly this is Direct (Connecting directly to the front face of the ADVC controller) and the communications port needs to be selected (this may be confirmed from the Device Manger within the Windows operating system).


Legacy KB System (APS) Data: RESL212729 V1.0, Originally authored by DaFr on 10/11/2013, Last Edited by DaFr on 10/11/2013
Related ranges: Others protection relays

AEDL3
Was this helpful?
What can we do to improve the information ?