Technical FAQs

Ask a Question

Write/Read Switchgear settings are greyed out in WSOS

In order to read and/or write switchgear files to/from an ADVC controller. The controller must be placed online. If the controller is in an offline state these features will be greyed out.


Legacy KB System (APS) Data: RESL212725 V1.0, Originally authored by DaFr on 10/11/2013, Last Edited by DaFr on 10/11/2013
Related ranges: Others protection relays

AEDL3
Was this helpful?
What can we do to improve the information ?