Technical FAQs

Ask a Question

What is the procedure for removing an ADVC controller from service for testings without tripping the recloser?

For unit removal without tripping the recloser: disable the trip and close switches located on the ADVC controller unit, power down DC, power down AC then disconnect the switchgear
Applying power for testing: power up AC, power up DC and test
Unit re-installation: connect switchgear, power up AC, power up DC, enable the trip and close switches


Legacy KB System (APS) Data: RESL212516 V1.0, Originally authored by DaFr on 09/17/2013, Last Edited by DaFr on 09/17/2013
Related ranges: Others protection relays

AEDL3
Was this helpful?
What can we do to improve the information ?