Technical FAQs

Ask a Question

Is it possible to remove the ADVC controller without tripping the recloser?

The ADVC controller was designed to be removed from service without tripping the recloser. To disable the trip upon removal, use the two switches located in the ADVC enclosure labeled Trip and Close then set them to disabled before removal.


Legacy KB System (APS) Data: RESL212515 V1.0, Originally authored by DaFr on 09/17/2013, Last Edited by DaFr on 09/17/2013
Related ranges: Others protection relays

AEDL3
Was this helpful?
What can we do to improve the information ?