Technical FAQs

Ask a Question

Sepam 20 series relay has additional I/O module outputs in red

The outputs must be activated. Connect to the relay using SFT2841, go to the Program Logic screen > click on Set Output Parameters > Set the output needed as YES in the used column.


Legacy KB System (APS) Data: RESL212482 V1.0, Originally authored by DaFr on 09/12/2013, Last Edited by DaFr on 09/12/2013
Related ranges: Sepam series 20

AEDL3
Was this helpful?
What can we do to improve the information ?