Technical FAQs

Ask a Question

Radio communications disabled when ADVC controller enters low power state

By default, when the ADVC controller enters the low power state the radio will be disabled after a programmable delay. To modify this setting such that the radio is not disabled, set the holdup time to 0. This may be modified from the front screen or via the WSOS software. To modify from within WSOS, open the switchgear file (or create it if necessary) click on Display > Radio Voltage > set the Holdup time to 0.


Legacy KB System (APS) Data: RESL212111 V1.0, Originally authored by DaFr on 07/22/2013, Last Edited by DaFr on 07/22/2013
Related ranges: Others protection relays

AEDL3
Was this helpful?
What can we do to improve the information ?