Technical FAQs

Ask a Question

Which SCEM card is associated with each series of recloser/sectionalizer?

N Series (up to 27kV) SCEM 11A
N Series (38 kV) SCEM 11C
U Series SCEM 11B
W Series SCEM 11D
RL Series SCEM 12


Legacy KB System (APS) Data: RESL211938 V1.0, Originally authored by DaFr on 07/01/2013, Last Edited by DaFr on 07/01/2013
Related ranges: Others protection relays

AEDL3
Was this helpful?
What can we do to improve the information ?