Technical FAQs

Ask a Question

What is the default port for connection to the ADVC controller?

The default port for communications is the the Null Modem RS-232 port. In order to communicate to the ADVC controller via USB, this must be changed to the ESB port via the FlexVue (front panel).


Legacy KB System (APS) Data: RESL211660 V1.0, Originally authored by DaFr on 06/04/2013, Last Edited by DaFr on 06/04/2013
Related ranges: Others protection relays
Was this helpful?
What can we do to improve the information ?