Technical FAQs

Ask a Question

Is it possible to connect to multiple ADVC controllers at the same time using WSOS?

Yes it is possible to connect to many different ADVC controllers at the same time. The controller that is listed in Bold is the active controller.


Legacy KB System (APS) Data: RESL211649 V1.0, Originally authored by DaFr on 06/04/2013, Last Edited by DaFr on 06/04/2013
Related ranges: Others protection relays
Was this helpful?
What can we do to improve the information ?