Technical FAQs

Ask a Question

Where may the ACE850 be configured?

The Sepam relay must be configured to accept the ACE850 before configuration of the device may occur. To enable the ACE850, connect to the Sepam relay via SFT2841 and select ethernet from the General Characteristics screen. Once ethernet is selected the ... box will be available to click. Click this box to open a menu allowing for the configuration of the IP, subnet mask, and Gateway information. Further configuration of the ACE850 may be done from the web interface for the module. To access the web interface, open Internet Explorer and type in the IP address of the ACE850, sign in and configure the necessary parameters.

Was this helpful?
What can we do to improve the information ?