Technical FAQs

Ask a Question

Is it possible to clear the alarm history within the Sepam relays?

It is not possible to clear the alarm history from the Sepam relays. The alarm history is only accessible via SFT2841 or ION/SPM.

AEDL3
 


Legacy KB System (APS) Data: RESL211123 V1.0, Originally authored by DaFr on 04/04/2013, Last Edited by DaFr on 04/04/2013
Related ranges: Sepam series 80, Sepam series 40, Sepam series 20
Was this helpful?
What can we do to improve the information ?