Technical FAQs

Ask a Question

How do I assign Sepam Equation Editor variables to output contacts?

The global equation editor variables (form of V1, V2, V3, NOT VL1, VL2, etc) may be assigned to the output contacts on the Sepam relay. It is possible that outputs O1, O4, and/or O11 (for Sepam 40 series) or O1,O5, and/or O101 will be grey due to CB control being set to on. The only way to assign the global variable to one of these contacts is to turn CB control off.

Note: Setting CB Control to off will disable the Circuit Breaker Control functionality of the relay.



Legacy KB System (APS) Data: RESL211078 V1.0, Originally authored by DaFr on 03/29/2013, Last Edited by DaFr on 03/29/2013
Related ranges: Sepam series 40, Sepam series 80
Was this helpful?
What can we do to improve the information ?