Technical FAQs

Ask a Question

Why is ANSI 46 trip C.B. feature not available for Sepam M41?

The Trip C.B. feature for ANSI 46 is only available if CB Control is set to ON.


AEDL3



 
Legacy KB System (APS) Data: RESL211038 V1.0, Originally authored by DaFr on 03/26/2013, Last Edited by DaFr on 03/26/2013
Related ranges: Sepam series 40
Was this helpful?
What can we do to improve the information ?