Technical FAQs

Ask a Question

Are collars available for the MiCOM P127 relay?

The factory is no longer manufacturing them, as such if one is needed it will have to be custom fabricated.


Legacy KB System (APS) Data: RESL210652 V1.0, Originally authored by DaFr on 02/14/2013, Last Edited by DaFr on 02/14/2013
Related ranges: Others protection relays
Was this helpful?
What can we do to improve the information ?