Technical FAQs

Ask a Question

How many point APS_SENSORS may be directly connected to the VAMP 321?

The VAMP 321 is capable of taking 10 point APS_SENSORS directly to the rear of the device.


Legacy KB System (APS) Data: RESL210597 V1.0, Originally authored by DaFr on 02/07/2013, Last Edited by DaFr on 02/07/2013
Related ranges: Others protection relays
Was this helpful?
What can we do to improve the information ?