Technical FAQs

Ask a Question

Does the VAMP 321 require a reboot if logic is input or modified?

If logic is input into a VAMP 321 the VAMP 321 will require a reboot. The reboot does not require a power cycle, it may be done directly from the VAMPset software.


Legacy KB System (APS) Data: RESL210596 V1.0, Originally authored by DaFr on 02/07/2013, Last Edited by DaFr on 02/07/2013
Related ranges: Others protection relays
Was this helpful?
What can we do to improve the information ?