Technical FAQs

Ask a Question

What is the maximum number of point APS_SENSORS that a VAMP 321 or VAMP 221 can monitor?

The VAMP 321 and VAMP 221 can monitor a maximum of 16 modules, using a 10L or 12L module you can monitor a total of 160 APS_SENSORS.


Legacy KB System (APS) Data: RESL210588 V1.0, Originally authored by DaFr on 02/07/2013, Last Edited by DaFr on 02/07/2013
Related ranges: Others protection relays
Was this helpful?
What can we do to improve the information ?