Technical FAQs

Ask a Question

What is the minimum Lux required for arc flash detection using a point sensor for a VAMP 321, 221, or 50 series relay?

A minimum of 8000 Lux is required for detection.

Was this helpful?
What can we do to improve the information ?