Technical FAQs

Ask a Question

Will the modules from a VAMP 221 work with a VAMP 321?

Yes, the modules will function with both the VAMP 221 and VAMP 321.


Legacy KB System (APS) Data: RESL210581 V1.0, Originally authored by DaFr on 02/07/2013, Last Edited by DaFr on 02/07/2013
Related ranges: Others protection relays
Was this helpful?
What can we do to improve the information ?