Technical FAQs

Ask a Question

How many APS_SENSORS may be connected to the VAMP 121?

The VAMP 121 is capable of monitoring up to 10 APS_SENSORS.


Legacy KB System (APS) Data: RESL210580 V1.0, Originally authored by DaFr on 02/07/2013, Last Edited by DaFr on 02/07/2013
Related ranges: Others protection relays
Was this helpful?
What can we do to improve the information ?