Technical FAQs

Ask a Question

Which Sepam relays support Cold Load Pick-Up?

Currently the relays that support Cold Load Pick-Up are:
-S24
-S50
-S52
-S53
-T24
-T50
-T52

AEDL3
 


Legacy KB System (APS) Data: RESL209936 V1.0, Originally authored by DaFr on 12/08/2012, Last Edited by DaFr on 12/08/2012
Related ranges: Sepam series 40, Sepam series 20
Was this helpful?
What can we do to improve the information ?