Technical FAQs

Ask a Question

What does SFT2826 do and where may I download the latest version?

SFT2826 allows the user to view any of the waveform captures from the Sepam relays. The waveform capture must be downloaded from the Sepam relay using SFT2841.

Nevertheless since the V14 SFT 2841 verson , you have to use tnow he Wavewin Softawre.



Legacy KB System (APS) Data: RESL209793 V1.0, Originally authored by DaFr on 11/28/2012, Last Edited by DaFr on 11/28/2012
Related ranges: Sepam accessories
Was this helpful?
What can we do to improve the information ?