Technical FAQs

Ask a Question

How to clear alarms using the front display for a Sepam relay.

To clear the alarms from the front screen:
1. Press the button with the triangle with ! in the center
2. Highlight List (defaulted to this) using the up or down arrow key
3. Press the reset (enter) key
4. Press the clear button

Note: This will clear the most recent four alarms, if more alarms are present the list and details options will still be available in the alarm screen. If all of the alarms have been cleared, only list will be available.


Legacy KB System (APS) Data: RESL209693 V1.0, Originally authored by MiZe on 11/17/2012, Last Edited by MiZe on 11/17/2012
Related ranges: Sepam series 80, Sepam series 60, Sepam series 40, Sepam series 20
Was this helpful?
What can we do to improve the information ?