Technical FAQs

Ask a Question

SFT2841 will not open after being installed on Windows 7 machine

The UAC controls will need to be disabled for SFT2841 to function properly on a Windows 7 machine. You may turn off UAC controls by the following:
Go to the Start Menu -> Control Panel -> User Accounts and Family Safety -> User Accounts -> Change User Account Control Settings and set to the lowest setting. Once this is done restart the PC.

AEDL3
 


Legacy KB System (APS) Data: RESL209129 V1.0, Originally authored by MiZe on 09/19/2012, Last Edited by MiZe on 09/19/2012
Related ranges: Sepam accessories
Was this helpful?
What can we do to improve the information ?