Technical FAQs

Ask a Question

64REF: Restricted Ground Fault is enabled but is showing as not recommended under the application screen.

Goals and Symptoms

64REF: Restricted Ground Fault is enabled but is showing as not recommended under the application screen.

Causes and Fixes

Issues:
The 64REF function will be enabled when you are monitoring either a single ground current or a single neutral current. However after enabling the 64REF protection function and you navigate to the application screen the 64REF will be listed as not recommended for use



If you are seeing this you will need to change the one line diagram listed under CT-VT APS_SENSORS.


Once the one line is correctly configured you will be able to navigate to the application screen listed under the protection settings and 64REF will be displayed as normal.



AEDL3
 


Legacy KB System (APS) Data: RESL208268 V1.0, Originally authored by MiZe on 05/30/2012, Last Edited by MiZe on 05/30/2012
Related ranges: Sepam series 80
Was this helpful?
What can we do to improve the information ?