Technical FAQs

Ask a Question

When attempting to open a waveform using SFT2826 receive an "Incorrect file name" error followed by a "This file cannot be open" error.

Goals and Symptoms

When attempting to open a .dat file for waveform viewing using SFT2826, the following errors are received:




Followed by:

Causes and Fixes

Navigate to the folder where your .dat and .cfg files are located. This location is determined when the files are saved.



Once the .dat and .cfg files are located change either the .dat or .cfg file name to match that of its corresponding file. Notice in the below example the .dat file has a .1 in it while the .cfg does not have the .1.



AEDL3



To resolve the issue in this example, simply add a .1 to the .cfg file or take the .1 out of the .dat file.

Legacy KB System (APS) Data: RESL208267 V1.0, Originally authored by MiZe on 05/30/2012, Last Edited by MiZe on 05/30/2012
Related ranges: Sepam series 80, Sepam series 60, Sepam series 40, Sepam series 20
Was this helpful?
What can we do to improve the information ?