Technical FAQs

Ask a Question

What do the most common Modbus Exception Error Code's mean?

Here is a list of the most common modbus error codes and what they mean.

Legacy KB System (APS) Data: RESL207784 V1.0, Originally authored by MaTh on 03/28/2012, Last Edited by MaTh on 03/28/2012
Related ranges: Ethernet and TCP/IP, Modbus / JBus
Was this helpful?
What can we do to improve the information ?