Technical FAQs

Ask a Question

Can the output associated with Zone Selective Interlocking on a SEPAM relay be changed?

No, the Zone Selective Interlocking (ZSI) output is preprogrammed into the SEPAM relay and is unchangeable. One is not able to use custom logic or LOGIPAM to change the output associated with ZSI either.


Legacy KB System (APS) Data: RESL205605 V1.0, Originally authored by MiZe on 06/23/2011, Last Edited by MiZe on 06/23/2011
Related ranges: Sepam series 20, Sepam series 40, Sepam series 60, Sepam series 80
Was this helpful?
What can we do to improve the information ?