Technical FAQs

Ask a Question

Does output 4 (O4) need to be wired for proper protection in SEPAM 20 and 40 series?

O4 does not need to be wired for the SEPAM 20 and 40 series to provide proper protection. O4 is used as a watchdog only. O4 acts as a malfunction detection output such that if a fault occurs in the relay it will be detected. The relay will then open the circuit breaker and enter fault mode.

AEDL3


Legacy KB System (APS) Data: RESL205509 V1.0, Originally authored by MiZe on 06/09/2011, Last Edited by MiZe on 06/09/2011
Related ranges: Sepam series 20, Sepam series 40
Was this helpful?
What can we do to improve the information ?