Technical FAQs

Ask a Question

What may SFT2841's Mimic-based UMI editor be used to do?

The Mimic-diagram editor may be used to:
1. Create a fixed bitmap background (128 x 240 pixels) using a standard drawing software.
2. Create animated symbols or use predefined animated symbols to represent the electromechanical devices or other objects.
3. Assign the logic inputs or internal status conditions that modify the animated symbols. For example, the logic inputs for the circuit-breaker position must be assigned to the circuit-breaker symbol to enable the display of the open and closed conditions.
4. Assign the logic outputs or internal status conditions that are activated when an opening or closing order is issued for the symbol.
5. Display the current, voltage, and power measurements on the mimic diagram.

AEDL3


Legacy KB System (APS) Data: RESL205508 V1.0, Originally authored by MiZe on 06/09/2011, Last Edited by MiZe on 06/09/2011
Related ranges: Sepam series 80
Was this helpful?
What can we do to improve the information ?