Technical FAQs

Ask a Question

In the equation editor in SFT2841, where do the inputs and outputs go in relation to the equals sign?

QUANTITYSide of Equals sign
Physical Inputs from MES RHS (Right Hand Side)
Protection Inputs LHS (Left Hand Side)
Protection Outputs RHS
Remote Control RHS
Input Variables RHS
Output Variables (Vx) LHS
Contstants RHS
Local (VLx) RHS or LHS
Local (VVx) RHS or LHS

AEDL3



 
Legacy KB System (APS) Data: RESL204889 V2.0, Originally authored by MiZe on 03/22/2011, Last Edited by MiZe on 04/20/2011
Related ranges: SFT 2841 - SFT2848 (Sepam series 20, 40, 80 software)
Was this helpful?
What can we do to improve the information ?