Technical FAQs

Ask a Question

How many data classes in the IEC61850 protocol are there and what are the subcategories?

There are a total of 355 data classes. The are divided into 7 categories as listed below:
Data Classes Number
1. System Information 13
2. Physical Device Information 11
3. Measureands 66
4. Metered Values 14
5. Controllable Data 36
6. Status Information 85
7. Settings 130

AEDL3
 
Legacy KB System (APS) Data: RESL204873 V1.0, Originally authored by MiZe on 03/19/2011, Last Edited by MiZe on 03/19/2011
Related ranges: SFT 2841 - SFT2848 (Sepam series 20, 40, 80 software)
Was this helpful?
What can we do to improve the information ?