Technical FAQs

Ask a Question

What does the IP filtering do in an ACE850 module?

By enabling the IP filtering in the module,it allows those specific IP addresses to access the module. The IP addresses can also be restricted to which module can access the ACE850. The different modules are ICE61850 and SFT2841 or both. This will provide a very secure webpage.

AEDL3


Legacy KB System (APS) Data: RESL204866 V1.0, Originally authored by MiZe on 03/19/2011, Last Edited by MiZe on 03/19/2011
Related ranges: Sepam accessories
Was this helpful?
What can we do to improve the information ?